Part Number: LP8866S-Q1 HI all,
I want to make sure something, right now I am checking the I2C LOG of the LED Driver 1. whether the placement is correct between the Brightness path diagram and the diagnostic register below?
And where is the correct path…
Part Number: LP8866S-Q1 Hi ALL
i have a question regarding the feedback resistor recommendation. What is 7~15 mean? is that the resistance or what?
Thank you
Part Number: LP8866S-Q1 Hi team,
In datasheet 7.3.6.5 Boost Output Discharge , it is described discharge duration is 400ms.
If customer power off early, e.g. Vin off after 150ms from EN = low, is there possibility of IC broken?
Also if there is something…
Part Number: LP8866S-Q1 Hi All
Right now i am checking the I2C Data result of LED Driver, using the I2C Reader tools, but when i got the result i cannot find the command of the write and read data on datasheet.
How to now what is the command or setting…
Part Number: LP8866-Q1
Hi,
can I use the LP8866 in “ Direct PWM Mode ”
with external PWM of 60Hz and any ״PWM input minimum on time” that is greater than 200nSec?
Part Number: LP8866S-Q1 Hi team,
My customer have question for 7.6.1.2 LED_CURR_CONFIG Register .
By this register setting, output current can reduce, does it? (e.g. 50 mA x FFFh(100%) = 50 mA)
Is there any precautions such as the duty being affected by…
Part Number: LP8866S-Q1 Hi Sir,
My customer has some questions about LP8866S-Q1, could it support the Luminous Intensity Minimum <2.5cd/㎡?
At this condition, the screen display does not have the jitters, flicker, or produce ripples or color casts. …