Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316C-Q1 , MCF8316A , Hello!
I've just purchased a new MCF8316AEVM expecting to get the new MCF8316C-Q1 chip installed because of this answer in FAQ site:
But the EVM has the old MCF8316A installed…
Part Number: MCF8316AEVM Hi,
I have MCF8316AEVM serious motor driver to drive drone bldc motors. Our bldc motor is 2900kv, max 10200 rpm, and max current is 5A. I couldn't drive that motor with EVM board.
I followed documents which are shared in the product…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MSP430FR2355 , MCF8316A Hi Team,
I have a fan design project, I use TI's MCF8316AVRGFR driver and MCU MSP430FR2355. So everything worked very well. However, when I set the mode change from forward…
Part Number: MCF8316AEVM Upon mistakenly loading the register set of MCF8316CEVM to MCF8316AEVM using Motor studio, brings the MCF8316AEVM board into some strange state, where it no longer communicate with PC. Even upon performing the Power reset and pressing…
Hi Bob,
For better transient, dynamic load conditions FOC based devices are preferable. The devices MCF8316C,15C, MCF8329A are range FOC devices where we can tuning Current Loop, Speed Loop PI gains to address dynamic conditions.
In the new GUI motor…
Part Number: MCF8316AEVM Hi
we can only turn on the motor once and then turn it off. Under normal circumstances, the motor cannot be used, and the fault alarm will be generated. However, the abnormal part cannot be used directly, and it cannot be read…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MSP430FR2355 I follow the steps below in the User's Guide MCF8316AEVM Evaluation Module information page.
7.1 Downloading Code Composer Studio and Importing MSP430FR2355 Interface Firmware …
Part Number: MCF8316AEVM Hello,
I am having some issues reading and writing to the EEPROM for the MCF8316AEVM. I can communicate to the board via the GUI but when I tried to run the MPET or the quick spin function, nothing happened. When I investigated…
Part Number: MCF8316AEVM I am using the MCF8316AEVM for product development.
I followed the Qucik guide in the datasheet exactly, but the 3-phase motor I connected doesn't move at all.
I can't even output any control signals. Can you tell me what…
Part Number: MCF8316AEVM I connect my motor exactly as it explained but it gives controller_fault when I run mpet or tried tu run motor by potentiometer.