Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A
Hi,
I have the eval kit setup such that the micro included on the kit is not connected to the MCF8316A, as I want to use my micro with it. I am scanning the I2C bus it is connected to…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A Hi,
I can successfully extract motor parameters using MPET: 2.4Ω, 1.8mH, 29mV/HZ. Manually enter the maximum speed: 240HZ.
Then IPD_T2_FAULT occurs when I give a speed via I2C, I…
Hi Annie,
Annie Liu said: Sometimes there will be a very large current, as if there is some force pulling it, if you don't let it go, it will stop falling after 3s;
When you refer to a force pulling it, do you mean that the current is increasing endlessly…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A Hi All, I have received my dev board today but I can't seem to get it to do anything. Using the installed and web gui I have been able to connect to the board but I am not able to read any…
Part Number: MCF8316AEVM Hello
On the GUI, on the Device and Pin configuration page, the first toggle switch (Speed pin config) is completely missing. There is no slide switch to toggle or select. The
next setting (External Pin..) has a selection switch…
Hi Linus,
Do you still require further assistance on this? Please help mark the thread as resolved if there are no further questions. Thanks.
Best Regards, Andrew
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A Hi Team,
Customer referred this thread: https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1044476/mcf8316aevm-connectivity-issue
A new development board…
Part Number: MCF8316A Hi,
I have successfully configured the motor and run it using I2C, now I want to control it with PWM, but nothing happens to the motor.
The settings in the GUI are as follows:
The input PWM signal is as shown in the figure below…