Rahul,
Did you ever over-write to the existing/factory programmed EEPROM? If so then there is a possibility of I2C target address to be overwritten. After clicking the "Find address" did the GUI report the correct I2C target address? Can you share the…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A I have the eval board and the latest version of the GUI installed. I open the GUI, close the first dialog box, as instructed, and the hardware connects, at the bottom of the GUI, it says…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A I am having the same issue as in this support thread , unfortunately the resolution was never posted there.
I went through the Guided Tuning process as described. Default settings are used…
Hi Vuong,
I've confirmed with our firmware engineer, and here are the answer:
Regarding current loop Kp/Ki:
These are user configurable Current Loop Kp and Ki
CLOSED_LOOP3.CURR_LOOP_KP
CLOSED_LOOP3.CURR_LOOP_KI
When the above CURR_LOOP_KP and CURR_LOOP_KP…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A , Hi,
Good Day.
We would like to try out the sinewave commutation of MCF8316A on a brushless motor.
We found an eval board MCF8316AEVM which has a GUI.
MCF8316A has 2 sinewave modulations…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A , MSP-EXP430FR2355
Dear community,
I would like to debug a simple Arduino software to Read and display on the Serial and to Write on the MCF8316A directly through I2C connected to MCx_SCL…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MSP430FR2355 Hello,
Section 7 of the MCF8316AEVM Evaluation Module User's Guide (sllu338.pdf) mentions a zip file with the firmware: “MCF8316AEVM_MSP430FR2355_Firmware_GUI.zip”
…
Hi Eric,
Eric Chen said: The source code of the I2C_read32() is contained within the main.c file of the CCS project that I've attached in my response above .
Example code to set the OVERRIDE bit and change DIGITAL_SPEED_CTRL to 10%, 53%, and 100%:
…