Part Number: MCF8316AEVM Using the MCF8316AEVM, the motor never gets into closed loop control. Instead, it locks into a random position. This is not braking, but rather maintaining torque at zero speed, thus consuming current.
I followed the steps of…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCT8316A , MCF8316A , MCT8316Z
Dear community,
During the tuning of the MCF8316AEVM, I found that when the PI controller is not well adapted, the motor under load is vibrating at a fix shaking frequency…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A I have a customer who wants Prime & Redundant MCF8316A controllers connected to the same low power motor (1 amp max current).
It does look possible by separately controlling the analog…
Hi Jonas,
If there are no more questions, could you please help mark this thread as resolved?
I will close the thread for now, but feel free to open it again if you have an additional question around this topic.
Best,
Robert
Part Number: MCF8316AEVM Hello TI experts,
I'm using MCF8316AEVM to drive a BLDC motor. Switches S1, S2, S3 are as per recommended Right , left, right position. Speed selection jumper is set to "POT" position.
When I'm going through guided…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A , MSP430FR2032 , MSP430FR2433 Ti Team,
We are currently developing Ceiling Fan Controller based on MCF8316A,
35Watt max, 24V Motor.
We will have following features,
IR Remote Interfa…
Part Number: MCF8316A Hi Team,
Have a good day!
My customer meets a question on the pin function difference between MCF8316A and MCF8316AEVM, mainly on Pin36-39. In MCF8316AEVM schematic, Pin36-38 is DACOUT and SOX, but in MCF8316A datasheet, Pin36,37…
Part Number: MCF8316AEVM While following the "Essential Controls" guide section of the GUI, I get a MPET_BEMF_FAULT after the motor twitches. This result is not consistent; occasionally other faults will be triggered, the MPET algorithm will idle forever…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A Hi All,
1. I downloaded the offline version of the GUI v1.1.8 and it behaves strange: It starts OK for the first time, works OK as well, however when I need to restart it, it shows logo…