Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A Hi,
I am using a MCF8316A EVM and currently tuning the device for the selection of motors that we use. During this process on a number of occasions the device reports "Closed loop aligned…
Hi Tanaka-san,
Glad to hear that you were able to spin up the motor after manually entering motor parameters.
Regarding Faster Deceleration - Step C, this is a typo in the GUI, even though the correct control widget [ACTIVE_BRAKE_BUS_CURRENT_SLEW_RATE…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A I have been spinning motors using the MCF8316AEVM board.
I designed a PCB with the MCF8316A chip and then hooked SDA and SCL to the EVM via the jumpers on the EVM. When I try to read…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A Hi team,
Here's an issue from the customer may need your help:
The evaluation board does not work.
After power-on, the GUI communication status is normal and the D6 cycle blinks. Read…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A Hello, I'm having issues spinning a specific custom motor with MCF8316AEVM.
To give you a small context, I was able to spin couple of other motors (powerful drone motors, like MK36…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCT8316ZTEVM , MCT8316AEVM Hello,
We have a customer here at DK, that purchased MCF8316AEVM and the box was labeled as such, MCF8316AEVM.
but inside the box was the MCT8316ZTEVM
are the boards…
Part Number: MCF8316AEVM After manually entering in the motor parameters (MPET seems to get them wrong), I'm able to get my BLDC motor spinning. I can play around with the various acceleration and other parameters and they seem to do as expected. However…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A Dear Team,
As per the application circuit mentioned in the datasheet of the MCF8316A, the nFAULT pin should be pulled up using 5.1kOhm resistor.
But in the Evaluation Board schematics…
Part Number: MCF8316AEVM I have finally been able to get a motor spinning (D2826 from amazon, just to play with and learn before connecting a more expensive motor).
The motor doesn't spin with the potentiometer fully clockwise. When I begin to turn the…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MCF8316A Hello,
I'm having trouble getting a motor to spin using the MCF8316AEVM. D1 and D4 are both green, ALARM and FAULT LEDs are both off. I have SW1 in the RUN position, S2 in the ABC…