Hi Megha,
I would recommend taking a look at the MCF8316C-Q1 which is AEC-100 qualified, can support 4.5 V - 35 V, 8 A peak, and Temperature Grade-1: -40C to 125C.
I would also recommend taking a look at the MCF8315A. This part is not AEC-100 qualified…
Hi Jordan,
For the CRC calculation, using this CRC calculator in CRC-8-ROHC mode: https://www.lddgo.net/en/encrypt/crc I was able to also get 0x5D when inputting "0x02 0xD0 0x00 0x84 0x03 0xc6 0xce 0x0f 0x44" which is how the MCF8316A will receive the data…
Hi Ruixin,
If the customer needs high accuracy of the motor position and cannot let the motor spin quickly at startup then a non-sensored solution may not be the best device. For low speed solutions that cannot have the startup have higher speeds we recommend…