Hi Adam,
Adam S said: Also, are parameters form Control Config-Motor Startup Stationary relevant for MPET? Changing align type can help?
While the startup method for MPET cannot be changed from Align, the current limit can. MPET will use the open loop…
Part Number: MCF8329EVM Tool/software: Hi, we are developing a medical device using a 24V BLDC motor (R=0,15ohm; L=0,12mH), peak current 10A. We managed to spin it with the EVM board and MPET without any load. The moment we applied a load appeared DRIVER_FAULT…
Part Number: MCF8329EVM Tool/software: Hi
I have the EVM unit connected to my motor. I am able to set it up via Motor Studio and get it running to 100% speed. I have followed a previous video posted by yourselves: MCF8329EVM_Getting_started. I have to…
Part Number: MCF8329EVM Other Parts Discussed in Thread: MCF8329A 이 보드로 BLDC모터를 제어하려고 하는데 첨부한 사진과 같이 MPET RESULT를 보면 Resistance 및 inductance 값을 기입할때 모터의 상저항인지 선간저항인지,
inductance는 모터 코일의 인덕턴스인지,모터 자체의 인덕 턴스인지 혹은 모터의 무부하 인덕턴스 값 중 어느값을 넣어서 모터를 돌려야 하는지 문의 드립니다…
Hi Jeong,
Updated download link here:
https://tidrive.ext.ti.com/u/_XR8pGh0fJDvdHyo/b75beb95-f9d9-44be-b770-9f14865dcd03?l
Access code: 6Nqyn$P6
Regards, Eric C.
Part Number: MCF8329EVM Other Parts Discussed in Thread: MCF8329A Hello,
I try to execute MPET as well with no result.
I'm running Motor Studio Version 0.1.15
This is a part of my log:
11:50:11:666 | :Beginning Motor Ke measurement...(Your motor will…
Part Number: MCF8329EVM Hi Team
Let me ask about HW_LOCK_ILIMIT.
When the cosutomer increase load to motor while the motor is spinning, an HW_LOCK_LIMIT error will occur.
There are two formulas for calculating base current depending on the data sheet…
Hello J,
Can you provide a capture of the phase current when MPET is running?
What is the max current rating of the motor? If the power supply is set to 1.5A then I assume this is close to the rated max phase current of the motor? If 1.5A is close to…