Part Number: MCF8329EVM Other Parts Discussed in Thread: MOTORSTUDIO , MSP430FR2355 Hello,
just got the MCF8329EVM and tryed to connect via USB with PC, but is is not detected by Motor Studio GUI SW.
I tryed many times to connect but no success, since…
Part Number: MCF8329EVM I have the EVM driving a motor attached to an electromagnetic brake for testing load conditions. When the motor is up to speed it easily handles the load even with the brake at it's maximum setting, but it has trouble starting…
Hi Marc,
The device does not have a way to notify or fault in the event of CSA output clipping. The best way is to directly monitor the CSA output on the SOx pin for any clipping.
Regards, Eric C.
Part Number: MCF8329EVM Other Parts Discussed in Thread: MOTORSTUDIO , , MCF8329A , MCF8316A In the MotorStudio software for the MCF8329EVM, Continuous Space Vector Modulation enable is grayed out. I also don't see it mentioned in the datasheet. Is that…
Hello Marc,
Marc Schuman said: Is it expected that I needed to adjust ILIMIT?
ILIMIT will limit the current that can be supplied to the motor to the set % of the value set in BASE_CURRENT. Depending on the rated peak current of the motor and the value…
Part Number: MCF8329EVM Other Parts Discussed in Thread: MCF8316A , , MCF8329A I'm trying to run MPET in the motor studio application, but I keep getting CONTROLLER_Fault and MPET_BEMF_FAULT with fault values, is there any way to solve it?
Hi Neil,
Sorry for late reply to this thread. I am looking into the thread now.
Few quick comments about the input.
We do not need to enter the R shunt in the GUI field. This version of GUI is initial version which require more updated .
Request to ignore…
Part Number: MCF8329EVM Other Parts Discussed in Thread: MCF8329A , MCF8316A Hello TI experts,
Great to finally see MCF8329 getting launched. I have questions as below:
1. MCF8329EVM page still shows description as MCT8329. I just want to make sure that…
Part Number: MCF8329EVM Other Parts Discussed in Thread: MOTORSTUDIO , MSP430FR2355
Hi support team.
I purchased MCF8329EVM. However, the GUI(Motorstudio) does not recognize EVM. I configured the hardware according to the user's guide, installed the GUI…
Part Number: MCF8329EVM Hi, I'm driving the motor with the MCF8329EVM and looking to get more detailed current information. The BUS_CURRENT looks good but is heavily filtered so I'd like to know what other information is available, I have several que…