Part Number: MCF8329EVM I was able to run MPET successfully, which moves the "next" cursor to the spin motor section however it is greyed out. Using the I2C controls in the sidebar also does not work. I'm able to read registers just fine so I think communication…
Hi Jeong,
Based on the register information you provided and assuming that the phase current shunt resistance (R44 on the MCF8329EVM) being used is 0.001mOhm We recommend changing the following current limits:
ILIMIT to 40%
LOCK_ILIMIT to 50%
HW_LOCK_ILIMIT…
Part Number: MCF8329A Other Parts Discussed in Thread: MCF8329EVM , MCF8316A I'm testing the MCF8329EVM in an application with pretty high load that engages quickly and often getting LOCK_ILIMIT faults. My motor is rated for peak currents of 78A, my BASE_CURRENT…