Part Number: MCF8315C-Q1 Other Parts Discussed in Thread: MCT8315A Is there a device that can directly control the amount of BLDC's 3-phase motor current? The primary chip is not required to process current, and the primary chip controls the speed directly…
Part Number: MCF8315EVM Other Parts Discussed in Thread: MCF8315A , , DRV8316 , MCT8315A
Dear support team,
I'm trying to use the GUI guide MCF8315A_GUI version 1.0.1 with no success,
In the Device and Pin Configuration section I cant find the Toggle…
Hello Venkatadri,
Thanks, you for response!
Few more questions we have to ask regarding suggested.
MCT8315A part is automotive grade? if not automotive grade please suggest AEC-100 grade.
MCT8315A part can drive fuel pump as per our voltage and current…
Hi Oben,
In terms of full BLDC integrated solution, including integrated control and integrated FETs, the MP6543H is most similar to the MCx8315A device. The MCT8315A includes a trapezoidal commutation algorithm while the MCF8315A integrates a FOC commutation…
Hi Ahmed,
We have many drivers in our MCx profile which are simpler to tune and offer a greater degree of control over the rise time.
I would recommend taking a look at the MCx8315 devices based on your required voltage and power level. The MCT8315A uses…
Part Number: MCF8315A Other Parts Discussed in Thread: MCF8316A , , MCT8315A , MCT8316A , MCT8316Z , DRV5055 Hi Dears,
1. The customer wants to choose the BLDC motor drive scheme, which is internally integrated with MOS. The motor specification is 12V and…
Other Parts Discussed in Thread: MSP-EXP430FR2355 , MCF8316A , MCF8316AEVM , MCF8315A , MCT8329A , MCT8315A , MCT8316A The MCx8xx family of integrated motor drivers contains registers and on-board EEPROM that can be interfaced and programmed using an external…
Hi Ben,
It seems like the main source of the confusion is the EVM schematic and not the datasheet itself. The EVM schematic is reused and slightly adapted for the MCT8316A, MCF8316A, MCT8315A, and the MCF8315A to help with our design efforts. The only…
In this E2E FAQ we will cover frequently asked questions about MCx devices in schematic and layout stages of design.
1. How should I configure the Thermal Vias on the BLDC motor driver device?
A common equation we use for the thermal resistance of vias…
In this FAQ we will cover some common faults that are triggered and how to resolve them by tuning the settings available on the MCx devices (with example pictures from the GUI).
1. MPET IPD Faults
A common fault we see with customers are MPET faults…