Part Number: MCT8316A Hi team,
As per the manual,
However, after writing 0x80000000 to the 0xE6 register, the parameters read are still the default parameters after power-up, and the previously modified parameters are not cured to EEPROM. Based on the…
Part Number: MCT8316A Hello, I would like to use the MCT8316A at approximately 160W. Is this too much power for the part? In the datasheet I see 12-35V operating voltage and an 8A peak output current capability. In my application we will supply the part…
Hi Yongsu,
Are you using the MCF8316A GUI? There is a possibility that there is a mismatch between the GUI target address and the actual device address (you can see that the communication above is to 0x1). If so, have you tried pressing the "Find Address…
Part Number: MCT8316A Other Parts Discussed in Thread: , MCF8316A Hi team,
Uses MCT8316AEVM to drive brushless DC motors and operates with adjustable switching power supply (29V supply, approximately 1.3A output current).
After debugging is good, run…
Part Number: MCT8316A Hi Team,
I encountered the problem of Loss sync when testing MCT8316. I can observe that the open loop is running normally, but the closed loop cannot be normal. You can check the waveform picture below,
I suspect that the current…
Part Number: MCT8316A Hi support team.
My customer has asked us about below.
Is there a way to write speed command information to EEPROM? We would like to rotate the motor without speed input after power on.
Best regards,
Higa
Part Number: MCT8316A Hi support team,
I have a question about the MCT8316A1V.
If the speed command is given by I2C and the sleep mode is not used, is it okay to leave the "SPEED pin" open?
Or should the "SPEED pin" be pulled up or pulled down…
Part Number: MCT8316A Dear Specialists,
My customer is designing the MCT8316A1V and has a question.
I would be grateful if you could advise.
---
I am designing a circuit for the MCT8316A1V and would like to know about the treatment of NC pins.
According…
Hi Andreas,
If there are no more questions, could you please help mark this thread as resolved?
I will close the thread for now, but feel free to open it again if you have an additional question around this topic.
Best,
Robert
Hi Goran,
If there are no more questions, could you please help mark this thread as resolved?
I will close the thread for now, but feel free to open it again if you have an additional question around this topic.
Best,
Robert