Part Number: MCT8316Z-Q1
Hello!
I am designing a motor controller using the MCT8316 driver, and would like to power the microprocessor using the motor drivers AVDD or buck regulator.
You show in Figure 9.1, a microprocessor being powered by AVDD, however…
Part Number: MCT8316Z-Q1 Hi team,
Could you help answer below questions?
1. What is the recommended frequency range for PWM input?
2. Voltage and current abs. range for FGOUT pin? And the delay time between HPx/HPn input and FGOUT output? Is the delay…
Hi Gokhan,
The MCT8315Z has ADVANCE angle (aka lead angle) configuration that ranges from 0 ° to 30° to accommodate the hall placement. This may require some trial and error tuning to achieve the optimal advance/lead angle setting.
Looks like this…
I'm planning to buy the MCT8316ZTEVM to couple with the hall sensors and see if it can drive our motor at low speed (~20rpm). According to your feedback, there is no need to test MCF8316C-Q1 anymore, but do you know where I can get the eval kit for…
Part Number: DRV10982-Q1 Other Parts Discussed in Thread: MCT8316Z-Q1 hi team,
can you help recommend a 3phase BLDC solution for control car display rotation? Detailed requirements as below:
need integrate M0
Lin interface (optional),
load current is…
Part Number: DRV5055 Other Parts Discussed in Thread: MCT8316Z , , TMAG5173-Q1 , TMAG5170 , TMAG5273 , TMAG5115 Hi Dear,
1.Our customer's application is UAV pan-tilt control. At present, MCT8316Z with control algorithm has been selected, and external Hall…
Part Number: DRV8312 Other Parts Discussed in Thread: MCT8316Z , MCT8316A , MCF8316A , DRV8316 , DRV8329 , DRV8328 , DRV8300 , DRV8306 , MCT8316Z-Q1 We are required to drive a 3 phase 24V, 3.1A BLDC motor. It is a sensored motor with hall effect sensors built…
Part Number: DRV11873 Other Parts Discussed in Thread: DRV10982-Q1 , DRV10983-Q1 , MCT8316Z-Q1 Hi team
Could you help give an automotive device with similar spec to DRV11873? My customer chosen DRV11873 on a prototype board and now the customer needs a automotive…
Part Number: MCT8316Z-Q1 Other Parts Discussed in Thread: MCT8316Z , MCT8316ZTEVM , DRV8316REVM Hi,
can internal buck converter or AVDD output in MCT8316Z be used for powering external support microcontroller without external nSLEEP pin control? On MCT8316Z…
Part Number: DRV8305 Other Parts Discussed in Thread: DRV8306 , DRV832X , DRV8343-Q1 , MCT8316Z , MCT8316Z-Q1 , DRV8304
e2e.ti.com/.../3963447
Sorry I have to come back on this thread that was locked now, due to me taking long. But I need it again.
"..…