Part Number: MCF8329EVM Other Parts Discussed in Thread: MCF8329A , MOTORSTUDIO , , MCT8329A I am trying to get a motor to run a bit faster than the top speed I'm currently achieving with the MCF8329A (at a fixed bus voltage). Preferably close to the…
Part Number: MCF8329EVM Other Parts Discussed in Thread: MOTORSTUDIO , MSP430FR2355
Hi support team.
I purchased MCF8329EVM. However, the GUI(Motorstudio) does not recognize EVM. I configured the hardware according to the user's guide, installed the GUI…
Hi!
As described in the FAQ, LED D7 lights up immediately after plugging in USB, so the EVM has the new MSP430 firmware.
We do not have a MSP430 LaunchPad available, and cannot use check or flash firmware onto the MCF8316AEVM.
On launching the MOTORSTUDIO…
Using MotorStudio, I have found by trial and error that if I pre-load the Motor Parameters in the settings page I can make the motor rotate. Yay!
but the MPET does not seem to be able to estimate or measure the MPET Results.
What would help is some kind…
Part Number: MCF8316AEVM Other Parts Discussed in Thread: MOTORSTUDIO Hi there,
I noticed the Errata #8, that the I2C can't read registers when the motor is spinning. And I've verified this point, that once we wrote the DIGITAL_SPEED_CTRL (0xEC…
Hi Joshua,
When you connect the MCF8315EVM to the computer which is LED D6 or D7 lit?
If D6 is lit then please try and use the Find Address feature in the GUI:
If this still is not working please check the voltages at pins AVDD, DVDD, VM, and CP. The…
Part Number: MCF8329EVM Other Parts Discussed in Thread: MOTORSTUDIO , , MCF8316A , MCF8329A I am trying to get a MCF8329AEVM working with a small 100W 10 pole motor running at 36V. Running the board standalone, the motor spins nicely, with speed controlled…
Hi Venkatadri
I downloaded the web interface again and there is no difference - no activity on the serial port. So I downloaded MotorStudio 0.1.9
I am seeing this error on startup:
however the app starts and I can connect to the board (D6 is now flashing…
Part Number: MCF8329A Hi
I am using GUI version 0.1.15.
EVM board and GUI art not connecting.
Looking at Device Manager, the USB driver is no installed.
Please share usb driver to connect EVM board to PC.
Regards.