Part Number: MPY634 Hello Guys,
Good day.
If using the MPY634 and tying both inputs to the same input signal...Vx = Vy = Vin, then should we expect Vout to be Vin^2 ? Will we see a reduction in noise at the output? will we see greater SNR at the output…
Part Number: MPY634 Other Parts Discussed in Thread: TMUX1112 Dear Sir,
We are looking for a Multiplexer such as AD633 and MPY634.
As a test result, we have a trouble in input Vos...
we need a precision accurate Vout for next amplifier, if there exists…
Part Number: MPY634 Hello,
I am using the MPY634 as an analog multiplier in the following configuration. I am having a hard time understanding the SF. In this case, the input voltage for both X1 and Y1 is 1.2V. For this input, I get an output of 0.35V…
Part Number: MPY634 Hello, I am using MPY634 as a divider. On the datasheet, it says that 'accuracy of the divider mode typically ranges from 1.0% to 2.5% for a 10 to 1 denominator range depending on device grade'. I don't understand what it means by…
Part Number: MPY634 I would like to use the MPY634 as a AM modulator. The circuit is wired exactly as mentioned in the datasheet figure 9 page 8.
Modulation input Em is + - 5V @ 150 Hz (square wave); Carrier input Ec= + - 8V @ 2 Khz (square wave) ; Power…
Part Number: MPY634 Can I know what would be the latency of analog multiplier MPY634 ?
Also can I multiply two signals of frequencies around 6GHz ?
Thank you.
Part Number: MPY634 We attempted to assemble a wide-bandwidth multiplier, using your MPY634 , but detected that its AFC was boosted with frequency (see table 1). Then we have assembled a test schematic in a prototype board with a M MPY634_TEST_01.docx M…
Part Number: MPY634 We attempted to assemble a wide-bandwidth multiplier, using your MPY634, but detected that its AFC was boosted with frequency (see table 1). Then we have assembled a test schematic in a prototype board with a MPY634 chip, just received…
Part Number: MPY634 Hi all Would you mind if we ask MPY634KP/KU? How much is the maximum TJ?(125C?) How much is the θja? We could not find it on the datasheet. Kind regards, Hirotaka Matsumoto
Part Number: MPY634 Hi team,
My customer is wondering if we have analog multiplier with single power supply, +Vs(eg 15V), -Vs 0V ?
Could you please help to answer this?
Thanks.