Dear Jens,
Can i check with you, what is the maximum number of samples per second when simultaneously sampling the 7 channels on MSP430F47177?
Thanks,Joy
Other Parts Discussed in Thread: MSP430F47177 , MSP430F5418 I use UART 0 and 1 to receive much data on MSP430 F2416. It worked perfect almost. But it corrupted sometime. Maybe lose one or two or three byte. Below list are my settings: Crystal is 4 MHz…
Aravind, The two microcontroller products that are included in the launchpad are these: * MSP430G2211IN14 – 2kB Flash, 128B RAM, 10 GPIO, 1x 16-bit timer, WDT, BOR, Comparator A+ * MSP430G2231IN14 – 2kB Flash, 128B RAM, 10 GPIO, 1x 16-bit timer, WDT,…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hi Paul,
I use the MSP430 product selection page from https://www.ti.com/microcontrollers-mcus-processors/msp430-microcontrollers/products.html and save all parts in the spreadsheet. I use the filters to filter out parts. There are quite a few that…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use the…
Hello Pavel,
EDIT: I didn't read past your first error. You already did this, and I didn't notice.
Pavel Hristov said:
We tried adding the following lines in io.h
#elif defined(__ MSP430F6726 __) #define __MSP430_6726__
For your first error…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave