Other Parts Discussed in Thread: MSP430F5244 , MSP-FET We are attempting to use the MSP-GANG430 to program boards via Spy by Wire. The controller on the board is the MSP430F5244. I have created a custom cable (12 in length, 4 conductor, 22AWG with mating…
Hi, James
James Evans said: . I'm checking to see if that errata applies to the MSP430F5249 or not.
In fact, the device to be commercialized is MSP430F5244.
Explaining the current situation in detail, the same phenomenon occurs in MSP430F5249 and…
Other Parts Discussed in Thread: MSP430F5244 , SN74LVC1G3157 Hi,
I want to use SN74LVC1G3157 in my application with MSP430F5244 mcu. In test circuit I have made connection between Select signal of
SN74LVC1G3157 to one of gpio of Mcu. When the mcu is power…
Other Parts Discussed in Thread: TXS0108E , MSP430F5244 I need to isolate my UART to USB bridge chip (FTID FT232RQ) from my MSP430F5244 so that power does not back feed in my circuit and cause the device to not shut down. I have 65 lines that power could…
Other Parts Discussed in Thread: MSP430F5242 , MSP430F5244 , MSP430F6433 , MSP-TS430RGC64C Hi,
I have problem with programming/reading/verifying/erasing MSP430F5242 with Elprotronic FET-Pro430 (programmer MSP-FET430IUF from Texas Instruments). SW return error…
Thank you
I use the msp430F5244 with 32KHZ XIN and 12MHz XT2IN so start up should be fine with low speed oscillator. After power up i would increase Vout up to 2.2V. However without any pull up or pull down I'm warried about TPS62742 stratup itself. Indeed…
Other Parts Discussed in Thread: MSP-TS430RGC64C , MSP430F5229 , MSP430F5244 , SYSBIOS Hello;
I have a project on which I've been doing development for a few weeks on the MSP430F5229 development board (MSP-TS430RGC64C), which uses Sys/BIOS. I haven't…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"