Part Number: MSP430F5329 Hi,
I have question about of UCS Module Fail-Safe Operation. We are facing the issue of increased power consumption due to UCS fail-safe operation. We are using XT1 operation ins LF mode, when a clock failure occurs in XT1, the…
Other Parts Discussed in Thread: MSP430F5329 HI All,
16 gb SD card interfaced to MSP430F5329 controller and read & write operations are Done.
now my doubt is without FAT file implement, is it possible to access SD card data through laptop, means what…
Part Number: MSP430F5329 Other Parts Discussed in Thread: CONTROLSUITE , , MSP-PMBUS I was able to find "PMBus Implementation Using the MSP430 USCI" and the SW. Unfortunately it is the code for a Master PMBus device. Of course my MSP430 is part…
Part Number: MSP430F5329 Not sure what I am doing wrong. But I am not reading the internal temperature correctly.
I am using the 2.5V internal reference and the ADC value I get is 1374.
Looking at the Device Descriptors and adc_ref15_30_temp 2051
adc_ref15_85_temp…
Other Parts Discussed in Thread: MSP430F5329 , MSP430WARE HI All,
16 SD card is interface to msp430f5329 controller and able to read and write data using SPI and also FAT32 file system write is tested, able to created text file on SD card and data is able…
Part Number: MSP430F5329 Other Parts Discussed in Thread: MSP430F5529 Hi community member,
In MSP430F5329 datasheet, "ESD Ratings" item can not be seen.
When the customer conducts the static electricity test of its own system, it seems that…
Part Number: MSP430F5329 I am looking at SLAU208P Revised October 2016. I am in the ADC12_A section 28.2.5.3 Sample Time Considerations Page 737. It says: The resistance of the source RS and RI affect tsample. The following equation can be used to calculate…
Part Number: INA169 Other Parts Discussed in Thread: LMP8645 , LM324 Hi,
So the issue is that when measuring with the ADC the gain of the INA169 will change according to the sample and hold time. As I understand this has to do with the fact that the INA169…
Part Number: MSP430F5329 Tool/software: Code Composer Studio Hi,
I am migrating a project. I got easily with the porting of some libraries but now I am facing a weird issue. The libraries are added on the include file and also precompiled (don't think…
Part Number: MSP430F5329 I am getting a XT1LFOFFG fault in UCSCTL7 At start I think I should get it because "After a PUC, the UCS module default configuration is: • XT1 in LF mode is selected as the oscillator source for XT1CLK. XT1CLK is selected…