Part Number: MSP430F6779A
Hi TI Support,
I suspect about connect capacitor with pin MCU of MSP430F6779A.
Which pin of the mcu if there is no connection to a capacitor? It will cause the mcu to not start-up.
Using 100-Pin PZ Package
Data…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest software…
Hi Akash,
The erase check and TX BSL version commands are members of the standard command set in BSLs V1.50 or higher but excluding 2.x BSLs. The MSP430G2544 is BSL Version 2.02, ergo no TX BSL version command support for this device.
You can go through…
Hi Paul,
I use the MSP430 product selection page from https://www.ti.com/microcontrollers-mcus-processors/msp430-microcontrollers/products.html and save all parts in the spreadsheet. I use the filters to filter out parts. There are quite a few that…
Other Parts Discussed in Thread: CC2640 , CCSTUDIO , CC2538 CCS not detecting installed compiler tools in Windows Docker container for CI build Hello all BACKGROUND: I'm trying to set up a CI build for a CC2640 processor using a Windows Docker container…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave