Part Number: MSPM0G1506 Hello,
I request you to provide IBIS model for MSPM0G1506SPTR LQFP (MCU). We are using this in one of our design where Tx, RX, CLK and Enable signal are used to communicate to isolators.
Thanks in advance for your help
Part Number: MSPM0G1506 Hello. I have two questions regarding the Total Unadjusted Error (TUE) of the MSPM0G1506.
1. Calculations were made based on the data sheet. Is the TUE correct at ±6.87LSB when using an external reference?
2. I would like…
Part Number: MSPM0G1506 Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
I need help with SPI (Motorola 3-wire with separate CS lines to 2 peripherals) on custom board. I'm sending data to my slave device but the received data on MISO…
Part Number: MSPM0G1506 Tool/software: The MSPM0G1506 is powered at an operating voltage of 2.2-3.0V. When VDD=2.2V, the output voltage value of the internal OPAMP decreased compared to when it was driven at VDD=3.0V. The OPAMP is used as an IV conversion…
Part Number: MSPM0G1506 Other Parts Discussed in Thread: SYSCONFIG Tool/software: I need to configure NONMAIN flash however using sysconfig is not ideal for my setup and I'm hoping for some alternatives. Doing it at runtime using self writes to flash…
Part Number: MSPM0G1506 Hi Team, my customer is using MSPM0G1506 in new project. customer meet inquiry below, please help to reply soon, thanks- Jerry
'Please help to suggest about the VREF+ whether need to connect VDD when use ADC function , I check…
Part Number: MSPM0G1506 Hello. My name is Mori. I'm looking for a way to measure internal VREF using an ADC. The calculation formula is as follows. Measure the internal VREF using VDDA as the reference voltage.
(Vref/VDDA)×4095 = measured value
If…
Part Number: MSPM0G1506 Hello Team,
my customer was wondering if need to consider the thermal vias in his layout. He will not run the MSP at full processing power.
thanks
Jan