Part Number: MSPM0G3107-Q1 Other Parts Discussed in Thread: SYSCONFIG Hi Team,
did I get it correct, that RTC_OUT (PA27 in my case) can only output 1, 256 or 512 Hz?
What would you suggest to do if I needed 32.768 kHz on an output pin? Is there a…
Part Number: MSPM0G3107-Q1 MCU: MSPM0G3107-Q1 Clock: Currently populated with a 16 MHz external crystal. We are evaluating whether it can be removed for BOM optimization. Interfaces: LIN (19.2 kbps), SENT position sensor, PWM-controlled LED dimming, GPIO…
Part Number: MSPM0G3107-Q1 TI part number: MOG3107QDGS28RQ1
Does this IC have an errata sheet? If not, reply: No.
If an errata sheet exists, were there any changes to the errata sheet during the most recent quarter (July to September)? If changes…
Part Number: MSPM0G3107-Q1 Other Parts Discussed in Thread: SYSCONFIG Please let me know if any mechanism is available for protecting the download over BSL. There is a password for BSL but this is in plain text right? Or is BSL expected only to be used…
Part Number: MSPM0G3107-Q1 Dear TI experts,
Could you check the rush current consumption of M0G3107QPMRQ1?
(for example, MCU will consump more current when it is in startup, or sleep/shutdown -> idle/normal status, etc...)
Where can I find this…
Part Number: MSPM0G3107-Q1 Other Parts Discussed in Thread: MSPM0G3107 This is a generic question regarding the MSPm0G3107 I want to implement Secure boot for the application software. How can i achieve this, especially since the MSPM0g3107 doesn't support…
Part Number: MSPM0G3107-Q1
Hi,
I am attempting to read the flash contents of the MSPM0G3107-Q1 (M0G3107QPTRQ1) device.
The setup has successfully connected once when an external resistor was added to the reset line outside of the board. However…
Part Number: MSPM0G3107-Q1 Other Parts Discussed in Thread: MSPM0L1228-Q1 Hi team,
I am currently evaluating the MSPM0G3107-Q1 (M0G3107QDGS20RQ1) for an automotive-grade project and wanted to know does the MSPM0L1288-Q1 support RTOS.
Thank you.
Part Number: MSPM0G3107-Q1 In the datasheet, it is stated:
"Standard with Wake allows the I/O to wake up the device from the lowest low-power mode of SHUTDOWN. All I/O can be configured to wake up the MCU from higher low-power modes."
Could you…
Part Number: MSPM0G3107-Q1 I am trying to receive packets of UART Data. I have configured the UART RX to happen via DMA. The transfer is also happening as expected. The failure use case is as follows: When a few bytes, say 1 or 2 bytes, are receved before…