Part Number: IWR6843AOP Other Parts Discussed in Thread: AWR1843AOP , DCA1000EVM Hello,
I am currently trying to use the IWR6843AOP with the DCA1000evm using mmWavestudio 2.1.0.0. I am getting the following error when I press the "SPI connect" button: "MSS…
Part Number: AWR6843ISK Other Parts Discussed in Thread: DCA1000EVM ,
Hello,
I am using the AWR6843ISK with the DCA1000evm and mmwave studio 2.1.1.0. When I try to connect to SPI, I keep getting a timeout error stating: [01:01:08] Status: Failed, Error…
Part Number: AWR2243 Tool/software: CPU information as follows:
gCLIMMWaveOpenCfg.frontEndCfg.csi2Cfg.lanePosPolSel = 0x35421
MmwDemo_openSensor start
Debug: CLI is operational
EDMAself_test[1] slavePowerUp success
MmwDemo_openSensor success
…
Part Number: CC2340R5-Q1
Tool/software:
Hello,
I am writting here regarding a problem experienced actually with CC2745R10_Q1 . Iam working with a demoboard and I am trying to configure in my application the device as a central . I start scaning, I can…
Hi
When I ported other people's sample code, the corresponding index value of the property table was incorrect, resulting in incorrect connect handle, so the app did not receive it。I fixed it myself
Part Number: IWR1642BOOST Other Parts Discussed in Thread: DCA1000EVM , , IWR1642 Hi,
I am trying to run IWR1642BOOST card with DCA1000EVM using mmWave studio. However I'm getting the error in the picture.
Here is the script messages if it is not shown…
Part Number: IWR1843BOOST Other Parts Discussed in Thread: DCA1000EVM IWR1843BOOST: MSS Power UP async event was not received
We are working with the mmWave Studio, and while we trying to do SPI connect we got RSP Time Out and a message "MSS Power UP…
I am currently working on the development of a driver for cascaded 2243 hardware, for which we are utilizing the mmWaveLink library. In the process of debugging, I have encountered an issue pertaining to the monitor function of the 2243 chipset that I…
Part Number: IWR6843ISK Other Parts Discussed in Thread: IWR6843 Dear All
I am using DCA1000 EVM + IWR6843 ISK with mmwave studio 2.1.1.0. version. while connecting to SPI it shows the following error, MSS Power Up async event was not received, the screenshot…
Hi Allison Nguyen,
Thanks for your reply.
I moved to an example SCI echo back to check whether I was receiving characters from the terminal or not.
The very first error I see in the example is given below:
Remember. Here SW1 is on (For UART to USB connection…