Part Number: ONET8501V Other Parts Discussed in Thread: ONET1151P , Dear Team,
For a thermal analysis my customer is asking for thermal resistance, maximum case temperature and T junction for components ONET8501V, ONET1151P.
We've noticed it doesn…
Other Parts Discussed in Thread: ONET1151L , ONET1151P , ONET8551T Hello,
Regarding:
TI Designs
ONET SFP+ 10G LR Reference Design With ONET8551T, ONET1151P, and ONET1151L
I am using a TI SFP+ Host Board (Rev. 2 2013 – 6572666) to communicate…
Part Number: ONET1151L Other Parts Discussed in Thread: ONET1151P , ONET8551T Unable to get chip to issue an acknowledge signal (drive SDA low). Attached picture of SCK (green) and SDA (yellow).
Hi JianYing,
This EVM is obsoleted and it is not provided any more. This EVM used ONET1151L plus ONET1151P and supported 10G-LR. Please refer to these two part's data sheet for more details.
Regards,, Nasser
Part Number: ONET8501PB Other Parts Discussed in Thread: ONET1151P , ONET8501P
Hi,
ONET8501PB and ONET1151P are offering some input threshold adjustments. But it is in digital form from 1 to 255 and there is no specification what exact range is covered…
Part Number: ONET8551T Other Parts Discussed in Thread: ONET1151P ,
Dear TI experts,
I was looking into this part in order to have a TransImpedance Amplifier from an external photodiode detector (FINISAR PhotoDetector). I was planning to have this…
Hi Wang,
Yes, you are right that the ONET1151P offers some amount of input equalization depending upon the input signal level using register 7; whereas the ONET8501PB does not. The other differences are:
1. The ONET8501PB is a rate-selectable limiting…
Part Number: ONET1191P Other Parts Discussed in Thread: ONET8501P , ONET1151P , ONET1151L Team,
Could you please help with the below question:
F or this project we want to amplify the signal delivered from an external fast photodiode amplifier of…
Hello Vincent,
I apologize for the very long delay on the reply. For very high speed TIA applications, we recommend the photodiode be as close as possible to the input of the amplifier to avoid parasitic such as inductance to cause instability to the…
Hi Lizon,
Yes, the ONET-10G-EVM comes with the 10G SFP+ module and the Host board as well. The only parts that the customer needs to have separately are the TOSA and ROSA which must be soldered to the SFP+ module (TI does not provide the TOSA, ROSA…