Part Number: ONET2804T Hi team
Could you help check the PCB layout and Bonding Diagram? If any potential question remain, could you help identify?
I attached the bonding diagram in attachment files. And I attached the PCB layout below:
RF side:…
Part Number: ONET2804T dear:
one of our customer need used ONET2804T on 100G Rosa, have to questions :
1. for the filter capacitor:
in the datasheet, It is recommended to use two single layer ceramic (SLC) capacitors in the range of 270 pF to 680…
Part Number: ONET2804T My customer used our TI-TIA ONET2804T in their ROSA, when they test RSSI, they got split in different voltage input, please check the plot:
It was tested in Rrssi at 10kohm: (marked red in the second figure), his questions are…
Part Number: ONET2804T The datasheet for the ONET2804T recommends 2 single layer caps between 270pF and 680pF to be bonded to the VCCI pads. If the ONET2804T will be mounted direct to the laminate and not to a ceramic substrate, can the VCCI connections…
Part Number: ONET2804T I am attempting to get the full datasheet for the ONET2804T TIA. The email address "onet2804t_request@ti.com" bounces back as undeliverable. How can I see the full datasheet and any reference design files? Thanks.
Part Number: ONET2804T I would like to order one of these parts in die form, but I need to know the pad pitch and pad layout (signal location on the die) on the die so I can design my test board for optimal wirebonding. Can anyone provide me that information…
Part Number: ONET2804T Hi,
I sent a request email about ONET2804T full datasheet to 'onet2804t_request@ti.com' (in ONET2804T brief Datasheet)
but I got the message that this email could not be delivered.
How can I get the ONET2804T full datasheet…
Hello Steve,
The ONET2804T was designed specifically to interface with a PIN diode with a 2.5V reverse bias voltage. The "Filter" pins self bias to this voltage and the pad spacing on the ONET die match with the pad spacing on several PIN diodes.…
Part Number: ONET8551T Other Parts Discussed in Thread: ONET2804T , LMH32404 , OPA855 , ONET8521T , LMH32401 Hi TI team,
It's William from best Epitaxy Manufacturing Company in Taiwan.
We'd like to adopt your TIA solution into our CPO platform design…