Part Number: ONET4201PA Other Parts Discussed in Thread: OPA855 , , ONET8551T We use PD+OPA855+ ONET4201PA to achieve optical wireless communication,OPA855 is single-ended output,How can OPA855 output connect to ONET4201PA? thanks.
Part Number: ONET4201PA Other Parts Discussed in Thread: SN65LVDS100 Hello, the ONET4201PA provides CML outputs, while our application requires LVDS signals. In order to provide the CML to LVDS translation, we can use the SN65LVDS100 (up to 2Gb/s). Do we…
Part Number: ONET4201PA How do you calculate the capacitance required for the optional external filter capacitor (coc)? I only see 2 values given (1) coc open = 25kHz and (2) coc 0.54uF = 0.8kHz.
Part Number: ONET4201PA Other Parts Discussed in Thread: ONET4251PA Thank you for your help.
Do you have an evaluation board for ONET4201PA or ONET4251PA? If there is, I would like to refer to the product information such as the model number. Could you…
Part Number: ONET4201PA Other Parts Discussed in Thread: DS125BR111 For my application I would like to use a multi level signal (PAM4) and I was thinking for the receiver to use an amplifier kind ONET4201PA as it has RSSI I can use it for output level…
Part Number: ONET4201PA Other Parts Discussed in Thread: OPA855 , , ONET8551T , LMH32401 Using the following two types of ICs,
I am trying to design an optical data receiving circuit that meets a communication rate of 1 Gbps.
・ OPA855
・ ONET4201PA
I…
Part Number: ONET4201PA I have a quick question: Is it possible to "compensate" for a wrong input polarity (DOUT+ of the input TIA goes to DIN- of the ONET4201PA and DOUT- is connected to DIN+) simply by pulling OUTPOL LOW or is this not the intended use…
Part Number: ONET4201PA We are currently seeing a 320 or so pico-second rise time on the copper transmitter signal @ 340Mbps.
The part says 80 pico-seconds max.
What are we doing wrong.
Please advise!