Part Number: ONET8501PB Hello,
I did a search for this in the forum search and it only came up with a post from 12 years ago simply stating that a model file was, at the time, not created for this product.
I just wanted to double check that one has…
Part Number: ONET8501PB Hello experts,
I have found an odd issue while using the ONET8501PB as the RX for an O/E application. During programming I set the pre emphasis settings on register 2 to a value of 8 (1000), which is not listed as a possible value…
Part Number: ONET8501PB Hi Experts,
Our customer wants to use ONET8501PB connected to ROSA with reversed differential input due to some layout optimizing issues, can you help to check is it OK for such using?
ROSA D- output connected to ONET8501PB DIN…
Part Number: ONET8501PB Other Parts Discussed in Thread: ONET1151P , ONET8501P
Hi,
ONET8501PB and ONET1151P are offering some input threshold adjustments. But it is in digital form from 1 to 255 and there is no specification what exact range is covered…
Part Number: ONET8501PB Hello,
Our customer use the ONET8501PB, have some question.
1) 2-wire interface
It is mentioned "Regarding timing, the ONET8501PB is I2C compatible" on the DS.
How about the input voltage level? Is it possible to use…
Part Number: ONET8501PB Hello.
We are looking for VCSEL driver solution for use with Finisar / HVS7000-004.
But Continuous current at inputs and outputs SPEC need up to 0.6 A~ 2.25A.
Do you have a suggest solution can provide to us? Thanks for kindly help…
Part Number: ONET8501PB Other Parts Discussed in Thread: ONET1151P Hi,
I'm comparing ONET8501PB and ONET1151P. I saw below statement for ONET1151P, so ONET8501PB does not have this register? Is this the main difference between these two parts?
These…
Part Number: ONET8501PB
Hi team,
My customer wants to know ONET8501PB default status of outputs and default output amplitude.
ONET8501PB has Dis pin and DIS register bit.
I have following 3 questions.
(1) Which one is given priority? Is it pin or register…
Part Number: ONET8501PB Hi,
I have an inquiry about your product, ONET8501PB. Datasheet indicates that there are 3 types of differential data output voltage and it can be controlled by registers, AMP0, AMP1. Then what is the default value of differential…
Other Parts Discussed in Thread: ONET8501PB , ONET8501V I want to use ONET8501V and ONET8501PB in an magnetic field (~0.3 to 1.5 Tesla). Will the chips still work properly? Is there any possiblity that the magnetic field will effect the parts' performance…