Part Number: ONET8551T Hello,
Prior to packaging, would would like to clean the ONET8551 with IPA and acetone. Are both of these safe to use on the ONET8551?
Thank you,
Nathan
Part Number: ONET8551T Hello,
I was hoping to learn more about the input impedance looking into the ONET8551T from the PD (so IN/FILTER). We are intending to first design a circuit to emulate the PD current for initial tests prior to connecting the…
Part Number: ONET8551T Hi Team,
In ONET8551T datasheet, we mentioned that
"For PIN diode applications, TI recommends grounding the BW0 pin. However, for higher bandwidth, the BW1 pin, or both the BW0 and BW1 pins, can be grounded. To reduce the bandwidth…
Part Number: ONET8551T Hi dear supporting team,
for ONET8551T, the d/s mentioned its sensitivity is -20dBm, while in the test report, it shows 20uVpp input current test result, which in calculation is lower than -20dBm, right? tks!
Hello Andrew,
Since you are inputting a photodiode current, it should work as expected in the figure. From Figure 10, it seems like even at 100uApp input current, the transimpedance gain should be at around 2kOhm to 3kOhm. Would you be able to describe…
Part Number: ONET8551T Dears,
For the ONET8551T , After APD TO-CAN burn-in,has 0.3% failure rate, Could you help to support that as below: 1.Would you support the reliablity report of ONET8551T ,including failure rate and working life; 2.The TIA need…
Hi Loren,
For the ONET8551T, After APD TO-CAN burn-in,has 0.3% failure rate,
Could you help to support that as below:
1.Would you support the reliablity report of ONET8551T,including failure rate and working life;
2.The TIA need burn-in?if yes,what…
Part Number: ONET8551T Hi Experts,
Our customer wants to know what's Small Signal Gain range for ONET8551T? We can not find this spec in our datasheet. Also, is the Gain related to the transimpedance value? For example, if the input small signal is…
Part Number: ONET8551T Other Parts Discussed in Thread: ONET8541T Hello, is there any evaluation board available for this part ONET8551T, assembled as shown in the Figure 17 (data sheet)?
Also, I wonder TINA spice macro is available.
Your feedback…
Part Number: ONET8551T Hello Team
can You comment on tha customer question:
Can we use Chip as RF signal amplifier without using input photodiode? We would like to use a 50 ohm source instead of a photodiode.
thanks and regards
Adrian