Part Number: ONET8551T Other Parts Discussed in Thread: ONET8501PB Dear All,
I see from the data sheet the ONET8551T has a differential output. I assume a differential amplifier would be needed to connect to the differential output and thereby suppress…
Part Number: ONET8551T Hello,
I am interested in a bit more information regarding the ONET8551T's pad layout. I completely understand that the device is designed for wirebonding, but we are planning to try flip chipping it to an interposer, which makes…
Part Number: ONET8551T Dear TI engineer,
We currently use TI ONET8551T produce optical communication module. Faulting rate is nearly 0.3% after burn-in. The TO burn - in conditions is as follows: 100℃,3.3 V voltage applied,24hr We would like to inquire…
Part Number: ONET8551T Our current APD-TIA ROSA failure is like this:
APD-TIA ROSA mounted in transceiver module with power on, the ROSA was damaged when a burst big input optical power (like 0dBm) into ROSA.
After failure analysis, we found the APD chip…
Part Number: ONET8551T I am using a detector based on photodiode + ONET8551T to measure the beat note between two lasers.
In our application the RSSI signal is loaded with a 10kohm resistor and 10pF capacitor and I would like to use the voltage signal…
Part Number: ONET8551T Dear Sir :
We have purchase ONET8501TYS and ONET8551TY, and we would like to purchase ONET8551TY die form as left picture , However the datasheet shows that the the ONET8551TYS4 and ONET8551TYS9 are supported by wafer , could TI…
Part Number: ONET8551T
Under the condition of different optical input power,when shutdown the input signal,there are different output waveform;as below
RX=-1.0dBm
RX=-5.0dBm
RX=-10dBm,
rx=-15dBm
Questions as follows
1.Under the condition…
Other Parts Discussed in Thread: ONET1151L , ONET1151P , ONET8551T Hello,
Regarding:
TI Designs
ONET SFP+ 10G LR Reference Design With ONET8551T, ONET1151P, and ONET1151L
I am using a TI SFP+ Host Board (Rev. 2 2013 – 6572666) to communicate with a plugged…
Other Parts Discussed in Thread: ONET8551T , ONET2804T Hi,
Can I check what is the storage temperature for ONET8551T? I can only find operating temperature support -40 to +100 deg C but not for storage temp in datasheet.
Main reason for asking is in the…