Hi,
You may want to take a look the ONET8551T. I'm not familiar with the requirements of an SDI signal, but that is our highest performing 12G capable TIA.
Regards,
Hi Vera,
In general I would suggest using a dedicated 10G device instead for that type of signal such as the ONET8551T. Is there a specific reason you are looking at using the ONET2804TLP for 10G signals?
Regards,
Part Number: TIDA-00088 Other Parts Discussed in Thread: ONET1131EC , ONET1101L , ONET1141L , ONET1151L , ONET8551T , ONET1151P Hi TI Experts,
I want to use TIDA-00088 to drive Laser Diode (P/N : LU0976M200).
But its operating current is 350mA, is there any…
Part Number: ONET4211LD Other Parts Discussed in Thread: ONET8551T , ONET1151P , ONET1151L , ONET4201PA Hello!
Can I get sfp module reference design on ONET4211LD or other driver for making 1G 1310nm sfp module with FP/DFB lasers?
Thank you!
Part Number: ONET-10G-EVM Hi,
Will the laser drivers used in this reference design function if driven with a 480Mb/s signal?
ONET1151L
11.3Gbps Low Power Laser Diode Driver
Optical Networking IC
ONET1151P
11.3Gbps Limiting Amplifier
Optical Networking…
Hi Janos,
Thank you for your interest in our ONET devices. My understanding is that you are using a VCSEL-based TOSA for your application- is that correct?
The TIDA-00088 and ONET-10G-EVM are reference design evaluation module/boards that are designed…
Other Parts Discussed in Thread: ONET2804T , ONET8551T Is the ONET2804T device suitable for use with either APD or PIN photodiodes (similar to the ONET8551T) or is it recommended for PIN photodiodes only?
Is there anything different in the design of devices…
Hi Lizon,
Yes, the ONET-10G-EVM comes with the 10G SFP+ module and the Host board as well. The only parts that the customer needs to have separately are the TOSA and ROSA which must be soldered to the SFP+ module (TI does not provide the TOSA, ROSA parts…
Hi Richard,
No, TI does not sell TOSA or ROSA components. The SFP+ module that you will receive along with the host board for this reference design kit includes the ONET1151L and ONET1151P devices. The customer is expected to attach their own TOSA component…
Hi Lizon,
Thanks for your interest in our parts.
1) The user guide and schematics come with the purchase of the EVM. If you have purchased an EVM and need the documents, please send an email to onet1130ex_evm@list.ti.com.
2) You could use the TOSA and…