Part Number: OPA810 Other Parts Discussed in Thread: OPA863 Hello,
According to datasheet of OPA810, this describes only spec for input impedance case of "common mode". On the other hand, case of another opamp (Ex OPA863), there are description…
Other Parts Discussed in Thread: TXU0101 , SN74AUP1G17 , OPA863 1MHz, 3.3v square wave (clock) with 50% duty cycle, can its amplitude be reduced to 2.7v using an op-Amp buffered powered with 2.8V single ended power supply?
Part Number: THS6214 Other Parts Discussed in Thread: THS6204 , , THS6062 , THS7002 , THS6002 , THS6301 , THS6302 , THS6222 , THS4561 , THS4551 , THS4541 , OPA2863A , OPA863 , OPA2863 , OPA810 Hi TI Team,
I search the receiver that can match with THS6214 or THS6204…
Hi Jason,
One other alternative I found that was within the 11V supply range requirement was the OPA863 but this is in our high speed catalog which has different performance specs and pricing accordingly. Note that to enable the amplifier, the shutdown…
Hello Michael,
That is a good point. I can not seem to find the original amplifier cross reference tool; it seems to have been replaced with this BOM tool. I did like the original one more as well, and will bring this up to the digital tool creation team…
Part Number: OPA365 Other Parts Discussed in Thread: LMV793 , SM73302 , OPA607 , OPA863 Hi team,
May I know if we have p2p replacement for OPA365AIDBVR or OPA365AQDBVRQ1? Customer is using OPA365 Q and non-Q part but facing supply shortage. I'm checking on…
Hi Rene,
There are not very many high voltage amplifiers with shutdown functionality so our options are limited. The only other devices I could find in the same package as the TLV2370 are the OPA863 and OPA734. But they do not have similar performance…
Part Number: TLV3541 Other Parts Discussed in Thread: TINA-TI , , OPA863 , OPA810 Hi Team,
I'm looking for oscillator solution that meets following requirement.
Vdd: 5V
freq: 400kHz ~ 1MHz (no adjustable requirement)
Vout_pp: 3~5V
low distortion.
I created…