Part Number: OPT3005 Hello Expert,
The most important specification is for selecting this part is what the tolerance is below 20lux.
Could you please share the data ASAP?
Best Regards,
Michael
Part Number: OPT3005 Other Parts Discussed in Thread: OPT3001 , OPT3006 , OPT3007 , OPT3004 Hi All,
I'm currently working with a Linux-based device on an ARM architecture, specifically running kernel version 4.9. I'm looking to interface an Ambient Light…
Hello Guillem,
Samples and evaluation modules (EVM) can be purchased online line. You can find links to the samples and EVMs on our product page here .
Rahland
Hi Dane,
We do not have any devices available in DIP packages. I would recommend the OPT3004 or OPT3005 depending on the customer's application. The OPT3005 is designed for video surveillance cameras, as it has 4+ orders of IR rejection that allow the…
Part Number: OPT3004 Other Parts Discussed in Thread: OPT3005 Hi team,
when using OPT3004/3005. the conversion time of OPT3004 or OPT3005 is configured as 800ms, is the photosensitivity reading obtained by one conversion based on the comprehensive environmental…
Hi Lumina,
OPT3004 provides an increased IR rejection than OPT3001. Furthermore, OPT3005 has the best IR rejection of the family.
In applications such as video surveillance cameras, where there is an IR LED used to illuminate the area when it is dark…
Hello Charlie,
The OPT3004DTS is a released device that has infrared rejection that is needed for video doorbell applications. However, the OPT3005 is a device especially made for the video surveillance applications which have increased IR rejection. …