Part Number: OPT3101 Hi Team:
In slau791.pdf,4.2.3 Per unit storing calibrating data in non-volatile memory;OPT3101 does not have non-volatile memory and needs calibration data to be stored in non-volatile memory. One option is to store these settings…
Part Number: OPT3101-SDK What debugging steps are recommended if the following error occurs in step 8 of the calibration routine (according to OPT3101 SDK Users Guide)?
The connections have been verified as follows: 3V3->J17.1, GND->J17.2, P4.1->J17.3,…
Part Number: OPT3101-SDK Other Parts Discussed in Thread: OPT3101EVM , OPT3101 , Tool/software: WEBENCH® Design Tools We use OPT3101EVM to dismantle MSP430, read phase and amplitude from I2C interface.
we set target distance is 0.2cm,but we get distance is…
Part Number: OPT3101 hi,
In the SDK OPT3101_Calibration.cpp file, there is Void OPT3101::device::calibrationSession_perUnitFactoryCalibration () method implementation, see "refDistanceInCodes = (refDistanceInMM[indx] * 4477) >> 10; ", some doubts, how…
Wenjuan,
I tested using Auto HDR mode, and tested using OPT3101 Configurator Tool to generate configuration files;My test is to open the SDK INLAB_STEP_0 conditional compilation, serial print amplitude, phase, temperature and other data
…
Part Number: OPT3101-SDK Other Parts Discussed in Thread: OPT3101 Hello Alex & Team,
This is continuation from e-mail thread.
*Unfortunately I don't have enough knowledge of software, I posted this inquiry on the e2e so as customer can directly comment…
Gordon:
1:Phase offset Ambient coefficient calibration is not to be done in a dark environment?
2:Is this calibration correct? After setting the distance between OPT3101 and the target, use the halogen lamp as the ambient light, adjust the brightness…
Gordon:
What I mean is that when I execute INLAB_STEP_1 in OPT3101 SDK, the calibrated phase offset parameters are saved in MCU FLASH. When I perform INLAB_STEP_2 step calibration, will the previous parameters in FLASH be erased;
I have another question…
Part Number: OPT3101 Hi expert,
Do we have sample code in C language that could be provided for us to better use OPT3101? The reference design and SDK are in C++ code. Thanks!
Joyce
Part Number: OPT3101-SDK Other Parts Discussed in Thread: OPT3101EVM I'm digging into the SDK with the OPT3101EVM. The SDK focuses on calibration which is very helpful, but I was wondering if someone could provide an example of how to used the SDK to capture…