Part Number: OPT4001 Tool/software: Hi,
We have got the OPT4001YMR in our production line, and our IQC feedback that there are some reflective foreign objects in the back of the device when we use the microscope;
Plesae refer to below picture and advsie…
Part Number: OPT4001 Hi team?
there is a simple question when using OPT4001, the calculation formula is (ADC_CORES* 312.5*E)-6, or ADC_CORES* 312.5*(E-6)? And where is the E value from?
BR
Jingguo
Part Number: OPT4001-Q1 Hi Expert,
I want to know if the device center is the sensor optical center. It determines my product structural design.
Regards,
Evan
Part Number: OPT4001 Other Parts Discussed in Thread: OPT3004 , OPT3005 Hi team,
do we have recommendation for below request?
dark current
< 0.05uA
Working wavelength
320~750nm
good inhibition effect on 850nm and 940nm
package
…
Part Number: OPT4001 Other Parts Discussed in Thread: OPT3002 From the datasheet:
8.5.1.1 Serial Bus Address To communicate with the OPT4001, the controller must first initiate an I 2 C start command. Then, the controller must address target devices via a…
Part Number: OPT4001-Q1 Hi team,
1. Could you please tell me INT output status at following register situation (always low?):
5-4 OPERATING_MODE, 3: Continuous
4-4 INT_DIR, 1: Output
3-2 INT_CFG, 2: Invalid
2. When INT_CFG is invalid, the behavior does…
Part Number: OPT4001-Q1 Hi team, could you kindly help on below two questions? Thanks!
1. The errors of different irradiation values are not found in the specifications. Is there any other experimental data? 2. After installing the product, error compensation…
Part Number: OPT4001-Q1 Other Parts Discussed in Thread: OPT3001 , OPT4001 Hi team,
I would like to enquire about the driver support for OPT4001-Q1.
Kindly let me know abt the drivers availability.
Part Number: OPT4001-Q1 Hi team,
According to the datasheet, the FOV is at least 35°, but there is a customer question that I need to confirm with you. The customer requires an FOV angle of about 45°. However, because the hole is too large, the…