Part Number: PCM1753-Q1 Other Parts Discussed in Thread: PCM1753 Hi team,
The BCK and SCK pins of the pcm1753 have an overshoot of 7.5V and a downshoot of -1V as below. Does it affect the device?
Hi Arash,
Arash Loloee said: Yes, the default is 24bit length, left justified.
Thank you for confirming this.
Arash Loloee said: The 2 plots above are not related to each other, correct? Because the colors are different for each waveforms.
The…
Part Number: PCM1753-Q1 Other Parts Discussed in Thread: PCM1753 , USB2ANY , Hello
Is it possible to use USB2ANY for controlling the PCM1753 by SPI?
Ito
Part Number: PCM1753-Q1 Dear TI Team,
Please help me with review of the below schematic and as well as help to share the circuit for LPF for both channels.
Part Number: PCM1754-Q1 Other Parts Discussed in Thread: PCM1753-Q1 , , PCM1753 , PCM1754 Hello Team,
I would like to know the difference between PCM1754-Q1 vs PCM1753-Q1.
I know the device comparison table show the difference. But is there any other…
Part Number: PCM1753-Q1 I want to know the range of the clock of MC pin.
I answered the other threads with 10KHz ~ 1MHz, is that correct?
It's 10 MHz to 1 MHz, but it's not a typo.
Part Number: PCM1753-Q1 hello, my customer will use 24kHz sampling frequency, and want to check if 12.288MHz master clock can be used. can you tell me if this is ok?
Part Number: PCM1753-Q1 Dear all,
one of my customer is trying to estimate the power consumption associated to the I2C portion of the PCM1753-Q1.
I know that it depends on the pull-up resitances, but is there any formula to estimate the Irms which…