Part Number: PCM1754 Other Parts Discussed in Thread: PCM5101 Hi team,
My customer would like to know, if TI has reference design of PCM1754.
I do not find any reference design in the TI.com,
Could team provide the reference design to my customer?
Part Number: PCM1754 Hello Team,
I would like to operate PCM1754 with non-common-audio related sampling frequency. (Except for 44.1kHz, 48kHz, 192kHz and so on.)
For example, In case of fs=70kHz, BCK= 64*fs=4.48MHz, and SCK=128*fs=8.96MHz, Can PCM1754…
Part Number: PCM1754-Q1 Other Parts Discussed in Thread: PCM1754 Hi,
We are using PCM1754 for Audio application.
I2S SCLK is set to 18.432 MHz
I2S BCLK is set to 768 KHz
and
I2S FS is set to 24 KHz
in datasheet Table 1. System Clock Rates for Common Audio…
Part Number: PCM1754-Q1 Other Parts Discussed in Thread: PCM1754 Hi,
We are using PCM1754-Q1 for audio application.
Circuit Details:
iMX8 (SAI) --> PCM1754-Q1 --> TAS5411 --> Speaker
PCM1754 is configured as follows:
Fs = 24 kHz
BCLK = 768 …
Part Number: PCM1754 Hey all, I was on this forum searching for "PCM1754 noise" and everything pointed to layout issues, grounding and decoupling. Although I had this exact issue seen in some posts, my resolution was none of the above.
At teh…
Part Number: PCM1754-Q1 Hi team,
Our assigned customer considers to use PCM1754TDBQRQ1 instead of PCM1754DBQR due to supply issue. I have questions about this.
1) Are these have same die? Or just a difference at test process and qualification process…
Part Number: PCM1754
Hi,
I am controlling the PCM1754 power(5V) though mosfet switch to control power up/down sequence. The same mosfet trigger signal is connected to mute pin of PCM1754 . If power ON and mute ON is triggered at the same time, is there…
Part Number: PCM1754 Hi,
I am controlling the PCM1754 power(5V) though mosfet switch to control power up/down sequence. The same mosfet trigger signal is connected to mute pin of PCM1754. If power of and mute ON is occurred at the same time, is there any…
Part Number: PCM1754-Q1 Hi team,
I have a question about unused output termination (VOUTL or R).
I plan to leave it open, but just in case if it radiate noise, I would like to terminate it to GND through the capacitor.
In that case, should I terminate…