Part Number: PCM1781 Other Parts Discussed in Thread: PCM1789 , PCM5242 , PCM1795 , PCM1742 Tool/software:
Hi TI E2E
Is it possible to obtain the IBIS model for the following component?
If it is not available, could you please let me know a close…
Part Number: PCM1781 Other Parts Discussed in Thread: TLV320ADC6120 Dear Expert
1. We connected a simulated MIC at pins 1 and 2, as shown in the following figure,
In a stationary state, i.e. without external sound sources, the waveforms of BCLK…
Part Number: PCM1781
Hi,
The customer is using a PCM1781 and says that there is a phase difference of about 46us (about 2Fs since the digital sampling frequency of the input is 48 KHz) between the VOUTL and VOUTR. Is this 2Fs within the normal operating…
Part Number: PCM1781 Other Parts Discussed in Thread: PCM1754 I am looking for a quick way to evaluate this PCM1781 (or the PCM1754). Is a dev board or evm available?
Part Number: PCM1781 Other Parts Discussed in Thread: PCM5242 , PCM1795 , PCM1742 Hello team,
The customer requested an IBIS model for the PCM1781?
If not, is there an IBIS model for a similar product?
Best Regards,
Akihisa Tamazaki
Part Number: PCM1781 When sampling clock and system clock frequency set lower than IC's recommended range , what problem occur this application?
⇒For example; noisy sound, sound clipped, IC is not power on, etc.
Request spec is below;
・Vcc: 5V…
Other Parts Discussed in Thread: PCM1781 Hello,
I want to convert audio data through the PCM1781 with the I2S bus, it is necessary to have the three clocks are synchronized, SCK (external oscillator: 24MHz), BCK (12 MHZ) and LRCK (192 kHz), and also…
Hi, Justin.
The PCM1781 can only operate as slave. So I need to send it 3 different clocks and the data has to be synced to them, no exceptions. So my mcu has to either receive or produce all of them. I can either use cpu generating clocks that maynot…