Other Parts Discussed in Thread: PCM1781 Hello,
I want to convert audio data through the PCM1781 with the I2S bus, it is necessary to have the three clocks are synchronized, SCK (external oscillator: 24MHz), BCK (12 MHZ) and LRCK (192 kHz), and also DATA…
Don,
I know it's been a while since this conversation started, but I'm beginning a new project and intend to use upgrade from the PCM1781 to the PCM5101A. The PCM5101A will be fed by a PurePath CC8520. From what I can see the I2S bus is the same, is…
Other Parts Discussed in Thread: PCM1781 , LM4860 Hello everybody.
I have made a design based on PCM1781 device which is giving me problems on some boards. Basically, the system is built up of a microcontroller connected to the PCM1781 by means of a I2S…
Hi Paul-san, Thank you for your understood that PCM1781(probably PCM1780 is similar as this) is similar device due to using same core but there isn't actual 2ch version.
Best regards, Kazuki Kuramochi
Other Parts Discussed in Thread: CC8520 , PCM5101A , PCM1781 I am currently designing a product with the PCM5101A which will be receiving data from a PurePath CC8520.
In the past I have used the PCM1781 but I'm upgrading.
My first question is about the…
I am measuring THD+N% on post DAC stage. I have isolated the THD+N% to PCM1804 by eliminating any other possibilities in signal chain. No I have not tried this on an EVM. I have PCM1808 for other sources on the board and for playback I have several PC…
Other Parts Discussed in Thread: TLV320AIC3204 , PCM1808 , PCM1781 , CC8520 Hey everybody,
There is a problem need help. I want to use CC8520 + ADC(PCM1808) as master, CC8520 + DAC(PCM1781) as slave. PCM1808 and PCM1781have no I2C bus, just use HW to control…
Part Number: WL1837MOD Hello
Our customers reported that they could not connect when using the wireless projection function(Screen Mirroring).
Is there any useful information in the attached log?
4532.messages.txt