Hi, the PCM 1795 documentation says it supports up to 192KHz input and 8x Supersampling. Does that mean the internal sampling rate of the filter can perform at 1536KHz? Perhaps there is a lower ceiling such as 384KHz, and the level of supersampling will…
Other Parts Discussed in Thread: PCM1795 , PCM1792A Dear Masters,
Can we support reference circuit for PCM1795 balanced output?
Thank you very much.
Eric Fu
Other Parts Discussed in Thread: PCM1795 , PCM1796 Hi team,
I have compared the user programm fuction control section of both PCM1795 and PCM1796 datasheet, it is almost the same except FMT[2:0] bit is different because 1795 is 32bit and 1796 is 24bit.…
Other Parts Discussed in Thread: PCM1795 Hello,
I can't find any CMRR/PSRR rejection for the PCM1795 DAC chip and I was wondering what is the worst acceptable power supply AC noise & ripple for the +3.3V and +5V voltages, peak-to-peak or RMS, measured…
Other Parts Discussed in Thread: PCM1795 Hello
My customer is using PCM1795 for thier CD-P several years for their products, and they intends to use for their 2015model also ,
However, recently, they found the THD had 7dB worsen(103 to 96.5dB(0.0015%…
Part Number: PCM1781 Other Parts Discussed in Thread: PCM5242 , PCM1795 , PCM1742 Hello team,
The customer requested an IBIS model for the PCM1781?
If not, is there an IBIS model for a similar product?
Best Regards,
Akihisa Tamazaki
Other Parts Discussed in Thread: PCM1795 Hello.
Regarding PCM1795 DAC, I want to know the Low ESR typed capacitors can be used as the decoupling capacitor for Vref. (VcomL, VcomR).
If not, please let me know why it is impossible to be used.
FYI, we found…
Other Parts Discussed in Thread: PCM1795 Hello, I 'm a new user of PCM1795 and this forum. I would like to use SPI to read and verify registers using Beaglebone black SPI, but the readback is unstable(readback word is not what was command to write)…
Other Parts Discussed in Thread: PCM1795 , PCM5242 Hi, TI Support Team
Customers are looking for substitutes for the following products.
Please recommend alternative products.
AK4490EQ / AKM
AK4493EQ / AKM
Thanks.
Regards,
MJ