Part Number: TAS6421-Q1 Other Parts Discussed in Thread: TPA3118D2EVM , PCM1808-Q1 I have now ordered an evaluation boards and a number of TAS6421. I want a robust way to convert my analogue data to digital for the TAS6421, it will need to operate between…
Part Number: PCM1808 Other Parts Discussed in Thread: PCM6240-Q1 Hi Sir,
I attached our audio DSP/AMP/ADC converter block diagram. The power in of the class D AMP is 20V, so the VDD of speaker out is 10V that is over the analog input power of PCM1808.…
Part Number: PCM1808 Hello to whom it may concern,
Our customer would like to use PCM1808 for monaural audio system.
In this case,
Q1, Can the PCM1808 use for monaural system?
Q2, If Q1 is OK, how do I handle unused input pins?
Q3, When it use for…
Part Number: TAS6421-Q1 Other Parts Discussed in Thread: PCM1808 , , TAS5421-Q1 The new problem is really to identify a way to connect a AQ100 (high temp) A/D converter to the TAS6421, with the minimal components as at temperature semiconductors become…