Part Number: PCM1820 Other Parts Discussed in Thread: TLV320ADC6140 , PCM1840 what's the real power consumption of PCM1820 and 1840 at 96KHz? The datasheet does not give a valid number.
Part Number: PCM1820EVM Tool/software: Hi team,
Here is MMFAE Chris. when my customer test PCM1820EVM, They have the question. detail as follow:
IN1 and IN2 connect to GND, and test output. Unusual test results:
pcm1820 NOISE TEST PPC3.approjx
Can…
HI
Wrong Part number! I just realised you sent me the link for the EU DoC of SKU PCM1820EVM whilst I need the EU DoC of SKU PCM1820 Q 1EVM
Can you please provide the EU DoC of SKU PCM1820 Q 1EVM?
Part Number: PCM1820Q1EVM Other Parts Discussed in Thread: PCM1820 HI
I had raised a question and closed it prematurely when I was provided a document not realising the document provided was not for the part on query here again:
Can you please provide…
Other Parts Discussed in Thread: PCM1820 Hello,
I'm very new to audio circuits. I want to record the sounds I receive from my microphones to the SD card. Is there an integration you would recommend for this?
Part Number: PCM1821EVM Other Parts Discussed in Thread: PCM1820 HI team,
My customer is evaluating PCM1820/21 EVM board. Their SDATA output is only 1V.
The settings are below.
FMT: L(I2S mode)
MSZ: L
MD1: L
MD0: L
MCLK= 12MHz
BCLK= 3MHz
FSYNC= 48kHz
Do you…
Part Number: PCM1821 Other Parts Discussed in Thread: PCM1822-Q1 , PCM1820 , PCM1820-Q1 If only one channel of the PCM1821 analog input pair is needed, what is the recommended connection for the other pair?
Does this same recommendation apply to PCM1820…
Hi Gerald,
Unfortunately the PCM1820 is hardware controlled an has a fixed 32-bit word length output. I recommend a software controlled ADC such as TLV320ADC5120 or PCM5120-Q1 that have a more flexible ASI that fits customer's project requirements.…