Part Number: PCM2704 Hello experts,
I'm researching the Power-ON/OFF behavior between VBUS and on-chip clock generatoer.
According to the result of waveform, the signal of output behavior was below.
Could you tell me the question below?
1) the…
Part Number: PCM2704 Hello experts,
I'm researching the Power down behavior between VBUS and external clock supply.
According to the result of waveform, the signal of output behavior was below.
Could you tell me the question below?
Question) the…
Part Number: PCM2704 Hi ti team,
PCM2704 displays USB AUDIO DAC after connecting to the computer, can this name be changed to the character name specified by the customer? thank you
Part Number: PCM2704 Dear team,
I kindly request you to provide alternate suggestions to PCM2704 as this device is NRND. We need the device with USB interface, also with longevity for next 10-12 years. Temperature Range from: -40 to +85/+1105/+125.
Part Number: PCM2704 Tool/software: Hello team, I need to design a circuit for USB to 3.5mm audio Jack for a project. I mostly heard that PCM series audio codec USB interface IC was used everywhere and still being used. I need a good suggestion with perfectly…
Part Number: PCM2704
Hi, I'm planning to use PCM2704 to provide a good audio output to a Linux based SoM ... I found a prebuilt adapter using PCM2704 working with this specific SoM but it has only headphone output (with no embeeded volume control buttons…
Part Number: PCM2704 Hi, TI Support Team
The customer wants to compose the circuit with the following blocks.
They are reviewing PCM2704 as a USB to Audio DAC during the block.
Can it be configured and used like the block above?
There does not…
Part Number: PCM2704 Hi Team,
My customer plan to use low cost micro-controller to driver the codec via I2C or SPI or USB interface instead of I2S.
Do we have recommended automotive grade part? Thank you.
Regards,
Roy
Part Number: PCM2704 I have some strange issue, may be somebody can decide what the reason.
I bought DIY board with PCM2704 (86M134M) and connect to laptop (Windows 7 64 bit, USB 2.0). Device was correctly recognized and driver was installed (USB\VID_08BB&PID_27C4&REV_0100&MI_00…
Part Number: PCM2704 What's the differences between PCM2704 and PCM2704C? please specific in Function
And if they are the function, please recommend me which one is better.