Part Number: PCM2900 Dear TI,
I'm the engineer from www.buckhorn.com.cn which develops professional usb sound card for PODcast.
We're using PCM2900 as OTG connected to mobile phone. But we hit one issue. PCM2900 reports input device as LineIN…
Part Number: PCM2900 Hi everybody! I use PCM290x series devices as a interface to Android smartphones through USB on the go. On most smartphones everything goes well, Android recognizes PCM290x chip and communicate with it without any problems but some…
Part Number: PCM2900 Other Parts Discussed in Thread: TLV320ADC5120 , TLV320ADC3101 , PCMD3140 , PCMD3180 Hi,
My customer wants to convert DMIC to USB. It can connect to PC as USB Microphone.
Do we have this kind of asic?
BR,
frank
Part Number: PCM2902 I have built an audio interface with PCM2902E. This worked perfectly with Android versions about 5 to 9 via an OTG cable, and with some earlier versions of Android 10. I thought perhaps the PCM2902 was too old to deal with newer OSs…
Part Number: PCM2900 The PCM2900 supports mic in and audio out.
Is there a way to set it for mic in only?
The audio (speaker) output should not be through USB for our application (mic in only).
Part Number: PCM2900C Other Parts Discussed in Thread: PCM2900 , Is the PCM2900, or any of its family chips capable of working with USB Type-C? I have just tried to use a Type-C cable but android devices do not recognize my device when attached. I used…
Part Number: PCM2900 Hello
I am facing an issue with the Vcom pin which is not able to deliver enough current. I am not using a lot ~ 100uA
I was wondering two things:
1) What is the maximum current I may sink from this pin.
2)May I provide to this pin…
Part Number: PCM2900 Hi I have a basic question.
I am designing a usb audio player circuit. Will this pcm2900 able to play a music file from a usb flash drive, with out a computer involvement.
I am expecting as soon as i plug in the u disc the music files…
Part Number: PCM2900 Other Parts Discussed in Thread: HID2
Hi
Our customer has found a failure sample at their board.
The phenomenon is that the beep sound can not be controlled (volume not be down).
Could you give us any advice what we should we confirm…