Part Number: PCM2903 Hi!
I am using the PCM2903 ADC to digitize measurements. So my question is whether the digital output of the ADC is a digitalization of the Voltage (Volt) or the Power (Watt)?
Since these are not proportional: P = V*V / R
Part Number: PCM2906C Other Parts Discussed in Thread: PCM2903 , The customer is considering to choose PCM2906C or PCM2903.
The customer find the below three advantages of PCM2906C.
1. The 2906 can use the internal 3.3V LDO as the power supply for VCCI…
Part Number: PCM2903 We've incorporated a PCM2903 chip into our board design and followed the reference design in the datasheet. It is connected to a USB hub chip which then goes to our microprocessor. We elected to provide an external clock source for…
Part Number: PCM2903C Other Parts Discussed in Thread: PCM2903 Hello team,
I want to use PCM2903C to achieve that LINE-in AUDIO INPUT, across the PCM2903C, then USB as output connect the Vehicle Head Unit play audio.
1. So can you help to comment if the…
Part Number: PCM2903 Other Parts Discussed in Thread: LMV796 I'm designing a circuit that is using the PCM2903 Audio Converter with a preamp built from the reference design TIDU765. When recording audio and playing it back there is a noticeable hissing…
Part Number: PCM2903
Hi,
I'm using this device to connect a headset + microphone but I'm having an echo problem. I set windows to voice recording and when I'm playing music and recording voice at the same time, the music is echoing to the mic input…
Part Number: PCM2903 Hi,
I'm using this part for Full duplex headset communication. Is anyone having a crosstalk problem where you hear yourself echo when speaking through the microphone? If yes, is there a solution to this issue?
Thank you.
Ni…
Hi Henrik,
I agree it would be strange. I'm about to start a test with your noise file.
As I was setting up I noticed that there are output buffers in between the output jack and the PCM2903 device. I know there aren't many convenient test points…
Part Number: PCM2903C Other Parts Discussed in Thread: PCM2903 , , OPA4353 , PCM2903EVM-U Hi there,
I'm running into an issue where the RCA output is not being detected on professional amplifiers such as Monoprice Unity and OSD XMP300. I checked with…
Part Number: PCM2903 Other Parts Discussed in Thread: PCM2912A Hi team,
My customer want to use the PCM2903 to connect the 2.75mm earphone with microphone and USB interface of CPU in server.
1. So can you help to comment if the PCM2903 can support to translate…