Part Number: PCM2903C Other Parts Discussed in Thread: PCM2903 , PCM2912 Hi there, I'm trying to integrate the PCM2903 with my Linux machine and I'm finding that it's not playing stereo audio out from the 3.5 mm jack. Instead it is blending it together…
Part Number: PCM2903C Other Parts Discussed in Thread: PCM2903 , PCM2912 , , PCM2912A Hi team,
My customer wants to use PCM2903 to do the function below.
We want to check when do the function, does it have some problems.
BTW: The customer uses PCM2912 before…
Part Number: PCM2903C Other Parts Discussed in Thread: PCM2903 Hi team,
My customer is evaluating the PCM2903 now and meets some problem.
When debug the PCM2903, they find the device has 18 altset. below.
Interface 2
Altset 1
Format: S16_LE
Channels…
Other Parts Discussed in Thread: PCM2903 , PCM2901 Hello,
I am currently working on a new design for which I plan to use the PCM2901 or the PCM2903. I need to know if these chips are fully USB audio class compliant (or in other terms they appear as "driverless…
Other Parts Discussed in Thread: PCM2903 , PCM2902 , PCM2903C Hi everybody,
I need the PCM2903's recording function for S/PDIF to USB conversion but the recording function does not work, neither analog nor S/PDIF. Playback works normal. In Options ->…
Part Number: PCM2903C Other Parts Discussed in Thread: PCM2903 Hello,
Below is my application:
Case1: CPU plays audio, SPK L and R can output simultaneously。
Case2:MIC1 input(VIN L), just SPK L has output, SPK R doesn't work.
Case3:MIC2 input(VIN R…
Part Number: PCM2903EVM-U Other Parts Discussed in Thread: PCM2903C , , PCM2903 Dear Specialists,
My customer is considering PCM2903C and confirming PCM2903EVM-U.
Could you please advise about their question.
---
I would like to evaluate the IC of PCM2903C…
Part Number: PCM2903EVM-U Other Parts Discussed in Thread: PCM2903 , PCM2903C Hi,
Is the IC that be mounted on EVM the PCM2903 or the PCM2903C?
Best REgards,
Kuramochi
Hello,
The PCM2903 is a hardware controlled device and a GUI is not needed to control the settings of the PCM2903. The on-board switches can be used to control the state of the HID and SEL hardware control pins. The EVM will enumerate like a standard…
Part Number: PCM2903C Other Parts Discussed in Thread: PCM2903 Hi team,
I was looking at the reference design for the PCM2903 Audio Codec, and the VIN coupling caps are electrolytic caps. Are these required, or can they be ceramic caps?
Thanks,
AH