Part Number: PCM3070 Other Parts Discussed in Thread: TLV320AIC3204 PCM3070 datasheet (SLA724A) page 7 says:
PLL Input Frequency max 20 MHz
However the datasheet page 22 says:
The PLL is highly programmable and can accept available input clocks in the…
Part Number: PCM3070 Hi team,
The read value of PCM3070 register is shown in the screenshot.
Page0 register 0x3F D6 has been set to 1 (Right DAC Channel Power up), but Page0 register 0x25 D3 is still 0, indicating right DAC power down.
PS: the read operation…
Hi,
Since we haven't heard back from you, we assume that you have found a resolution. I shall close this thread. Please reply to this in case you have further queries on this.
Best Regards.
Part Number: PCM3070 Hi teams
This is Gabriel Xu from South China OEM team, my customer is using PCM3070 in new design and they need to use headphone output function.
The input signal is single ended from IN1L and IN1R, and the output pin is HPL and HPR…
Part Number: PCM3070 Other Parts Discussed in Thread: TLV320ADC3101 , PCM1804 Hi,
I am considering using the PCM3070 and other devices which also include the miniDSP capability for use in a Pro Audio system design. However I have some rather unusual signal…
Part Number: PCM3070 Hi teams
My customer encounters an abnormal phenomenon during using PCM3070.
Customer supply LDO IN with 3.3V voltage, disable DLDO through LDO_select pin and disable ALDO through register.
They supply AVDD & DVDD and IOVDD with 1…
Part Number: PCM3070 Dear, Sir.
The datasheet expalnes the LOL & LOR will be used for Stereo Line Output.
The othher side, DAC Stereo SE Line Output performance are separated 2.
Does it maen HPL & HPR can be also used for Streo SE Line Output?…
Part Number: PCM3070 Other Parts Discussed in Thread: OMAP-L138 Hi, I am bringing up a new HW design with a PCM3070. The codec is coupled to an OMAP-L138 McASP and successfully streaming wav files with aplay, but still working on getting audio capture…
Part Number: PCM3070 Other Parts Discussed in Thread: TLV320AIC3212 Hi, Looking at the PCM3070 I understand that it has multiple I2S ports. In a previous discussion on this forum and also with reference to the application note regarding this fact; it…
Part Number: PCM3070RHBEVM-K Other Parts Discussed in Thread: PCM3070 Hi,
Our customer used PCM3070 and encounter usb setup issue (Use Win7 system) as attached file.
Have any suggest to overcome it.
Warm Regards,
Lin