Part Number: PCM5102A-Q1 Other Parts Discussed in Thread: PCM5102 Hi expert,
In the layout of PCM5102, can I seperate AGND and DGND into two different GND? May be its better to reduce noise from DVDD?
Part Number: PCM5102-Q1 Other Parts Discussed in Thread: PCM1753-Q1 , PCM1789-Q1 Dear all,
one of my AA, would use the sample rate fs=20.5KHz, but this is not allowed in neither 3-wire and 4-wire mode.
Is there any other Automotive Audio DAC which supports…
Other Parts Discussed in Thread: PCM5102-Q1 , PCM5122 , PCM5102 , PCM1794A Hi,
Can the PCM5102-Q1 Audio DAC generate stable DC output? In the intended application, we need a variable frequency (DC to 10kHz) sinus output.
Thanks for your help!
Best regards…
Part Number: PCM1754-Q1 Other Parts Discussed in Thread: PCM1754 , PCM5102 Hello,
does it support 16-bit(not 24-bit) i2s?
i'm porting the pcm1754 to an embedded linux system.
and it is set to I2S 16bit mode but it didn't work.
but i connected to…
Part Number: PCM5102A-Q1 Other Parts Discussed in Thread: PCM5102A , PCM5102 , PCM5122 Hi team,
Older version, PCM5102 (non A), has following specification for BCK but it is not in the datasheet of PCM5102A(-Q1). Is the BCK specification of A and non A same…
Part Number: PCM1789-Q1 Other Parts Discussed in Thread: PCM1789 , PCM5102-Q1 We would like to use #PCM1789 as replacement for Analog Devices part # AD1859 ? Is this a good option? Or any other good suggestions to replace with?
Part Number: PCM5102A-Q1 Other Parts Discussed in Thread: PCM5102-Q1 , PCM5102 Hi,
I would like you to confirm Power Sequence about PCM5102A-Q1. I understood that user can separate DVDD and AVDD/CPVDD.
My customer try to supply DVDD and AVDD/CPVDD separately…
Hi Justin,
Thanks for choosing the E2E! Regarding the parts you are looking for, here is my recommended solution:
PCM5102-Q1
Operating temp range: -40 to 105C
TI page: http://www.ti.com/product/pcm5102-q1
Input: I2S
There is also EVM board for the part …
Part Number: PCM5142 Other Parts Discussed in Thread: PCM5102 , PCM3070 , PCM5102A , TLV320AIC3254 ,
Hello
My customer choosen PCM5142 for next project.
However, they hope to use miniDSP and also have flat responce 10Hz~40KHz +/-1dB.
Would please let us know…