Hi Raphael Xu,
Do you have driver specific to PCM5242 DAC?
In most of the forum, I came to know that PCM5142 and PCM are almost similar , even their Register Mapping is same.
So, can we use below driver files for the PCM5242 audio DAC ?
sound/soc/codecs…
Part Number: PCM5121 Other Parts Discussed in Thread: PCM5141 , PCM5122 , PCM5142 Hi Team,
Due to the shortage of PCM5121, can we used PCM5141 to replace it? I found out that they are P2P, also according to the E2E post below, PCM5141 provide the addition…
Hi Liu,
I spent some time today with the PCM5242 EVM and Purepath Console 2. I wasn't able to get the SDOUT linked to the volume control registers
from a little searching it seems like this is the intended way to link the volume control in PPS https…
Part Number: PCM5121 Other Parts Discussed in Thread: TLV320ADC3140 , , PCM5141 Our application has a custom bit rate (near 32khz), without master clock.
Internal PLL lock the frequency and the system works.
Now we need to use the fixed flow dsp for equalization…
Hi Wiky,
It is not possible to route the mono-mix to the analog output in the PCM5121. The best you can do is play both channels as left or right data.
This is possible with a customer process flow on the PCM5141.
Thanks,
Paul
Part Number: TAS5755M Other Parts Discussed in Thread: PCM5141 , DRV612 , PCM5121 , DRV604 I have a design based on TAS5755M Amp in a 2.0 BTL 50+50W configuration.
The client would like to add line-out to this device now too. Should I just multiplex the I2S…
Part Number: PCM3070RHBEVM-K Other Parts Discussed in Thread: PCM3070 , PCM1870 , PCM5141 , PCM5122 , PCM5142 , PCM5121 Hi,
I have a PCM3070EVM-K and am attempting to get PurePath Studio to download code to it. A popup box says
Warning: This board has an invalid…
Hi, Kes,
Unfortunately, the ROM of the PCM5121 cannot be modified and the I²S output is fixed to mono as it is intended to be used for applications requiring a subwoofer. If a custom configuration is required when I²S out should be stereo according…