Hi, Kes,
Unfortunately, the ROM of the PCM5121 cannot be modified and the I²S output is fixed to mono as it is intended to be used for applications requiring a subwoofer. If a custom configuration is required when I²S out should be stereo according…
Other Parts Discussed in Thread: PCM5242 , PCM5142 , PCM5141 , SRC4392 Hi team,
1. I used PPS(home audio) to control PCM5242 EVM,but I can only select PCM5142 from frameworks. does it work if I select PCM5141?
2. I connect a simple circuit to test whether…
Hi Ilic-san,
I would suggest the following parts.
- TAS5548/58(PWM Modulators) & TAS5614LA/24A(Power Stages) - PCM5121/2, PCM5141/2, PCM5242(Audio DACs) & TPA3116D2, TPA3245, TPA3250, TPA3251, TPA3255(Power Stages)
Best regards, Kato
Part Number: PCM5142EVM-U Other Parts Discussed in Thread: TLV320AIC3262EVM-U , TLV320AIC3254EVM-K , PCM5141 Hi,
A customer asks to us about an error message of PurePath Studio(Home Audio) using PCM5142EVM-U. The error message is as follows;
Error: MiniDSP…
Other Parts Discussed in Thread: PCM5141 , PCM5121 I have a customer planning to use PCM5141 for basic volume control and equalization so they plan on using the default ROM mode (not pure path). Are there any reference code/software that has the registers…
Other Parts Discussed in Thread: PCM5141 Hi I have just been granted access to the PurePath Studio platform. I am hoping to use it with a PCM5141. Unfortunately when I install and run the program I get an error citing some missing xml files. It appears that…
Other Parts Discussed in Thread: TLV320DAC32 , PCM5121 , PCM5141 , PCM5142 Hi, I am using a TLV320DAC32 with an external MCLK input and I want to continuously vary MCLK on the fly while it its playing audio over a wide range e.g. a 4:1 frequency range to achieve…
I posted the question below a month ago. It has had 51 views but no replies from TI or anyone else. Could Don Dapkus or someone else please reply to my questions below, even if the answer is no - there are no DACs that can do that. - Thanks.?
Hi, I am using…
Other Parts Discussed in Thread: PCM5142 Hi,
Just new to PurePath and the miniDSP engine on the TI chips, and am having some issues.
I created a very simple DSP filter, that just switches the left and right channels from the input to the output. I then…