Part Number: PCM6360-Q1 Hello,
I'm evaluating the PCM6360 for an automotive audio application (multi-channel input stage for a DSP-based amplifier, no microphone) and I have a question regarding the MICBIAS architecture.
In my design, multiple input…
Part Number: PCM6360-Q1 Hello,
My customer is asking about active noise cancellation(ANC) in PCM6360-Q1(PCM6xx0-Q1).
Is it possible for this device to perform ANC processing on its own?
Or are other MCUs or processors required for ANC processing…
Part Number: PCM6360-Q1 Hi team,
What should we read when interrupt signal is triggered?
If we receive an interrupt signal, we should read:
0X27 - 0X33 register, to check diagnostic;
0X35-0X37 register, to check over voltage and MICBIAS fault;…
Part Number: PCM6360-Q1 Other Parts Discussed in Thread: TAS5825M I am trying to implement a 5ch audio system with monaural output. All inputs a line level AC coupled single ended. Each channel requires a digital volume control from mute to full volume…
Part Number: PCM6360-Q1 Tool/software: Hi team,
When my customer was testing the microphone input, they observed that as the microphone input decibel level increased, the output suddenly dropped from the maximum value to the minimum value. They would…
Part Number: PCM6360-Q1 i have two questions regarding the use of the pcm6350 input configuration and diagnostics .
if using the 6360 for line inputs with 3pin jack connectors tip connected to Positive input and ring connected to Negative input on…
Part Number: PCM6360-Q1
Tool/software:
Hi epert,
I want to ask a following question related to this thread:
PCM6260-Q1: For MIC+ line shorted to battery fault; any potential risk on V_MICBIAS? - Audio forum - Audio - TI E2E support forums
In…
Part Number: PCM6360-Q1 Tool/software: Hello Team.
What is the resolution of the internal ADC?. It is mentioned as multibit delta-sigma ADC.
I have requirement which asks for 24-bit ADC, does this part support it?
Part Number: PCM6360-Q1 Hi Team,
The maximum output current of MICBIAS in PCM6360-Q1 is only 80mA. Customer needs 120MA max Current.
Can customers use other power supplies as the bias voltage of MIC instead of using the MICBIAS voltage supply of…