Part Number: PCM6360-Q1
Hi team,
Our customer have a question about the PCM6360-Q1.
The Input Line in is the 1kHz signal source, and the output is output disconnected.
As the pictures shown, the yellow is output and the green is input.
The content of the…
Part Number: PCM6360-Q1 Other Parts Discussed in Thread: PCM6260-Q1 Hi team,
My customer need to modify their schematic due to the shortage of PCM6360-Q1 and they move to PCM6260-Q1. The following is part of their schematic and they use MICBIAS=9 V. I'd…
Part Number: PCM6360-Q1 Other Parts Discussed in Thread: PCM6260-Q1 Hi Expert,
I would like to know
difference between PCM6360-Q1 and PCM6260-Q1
can I use 6260 to replace 6360 due to the shortage
Thanks for help!
BR,
Elec Cheng
Part Number: PCM6360-Q1 Other Parts Discussed in Thread: TAS6424E-Q1 , TAS6424E Hi team,
One of our customers questions:
When designing the TDM interface, I would like to share FS/BCLK with the TAS6424E-Q1 to be connected to the DSP. The TAS6424E is configured…
Part Number: PCM6360-Q1 Hi, team,
Some questions about PCM6360-Q1 in customer project.
Below is connection diagram. SOC TDM2 is CLK master, other devices are slave, including SOC TDM4 and ADC PCM6360-Q1.
When SOC TDM2 is master and SOC TDM4 port is…
Part Number: PCM6360-Q1 Hi,
I'm looking at PCM6360-Q1 I don't expect to use the microphone bias circuitry and the diagnostic. If I don't use these do I then need to supply HVDD and VBAT_IN? If not, should they the be left floating or connected…
Part Number: PCM6360-Q1 Hi Expert,
Our customer use PCM6360-Q1 in their project. Now as you can see below sentence from its datasheet, it says it supports multiple-cycle-width bits clock. If I understand right, this usage should be the red line as below…
Part Number: PCM6360-Q1 Other Parts Discussed in Thread: PCM6340-Q1 I am using the PCM6360, quite happy with it. Just have the problem, when I apply no signal, the FFT shows noise floor at about -140dB, but some peaks at random positions, which are chip…
Part Number: PCM6360-Q1 Other Parts Discussed in Thread: PCM6260-Q1 , PCM6240-Q1 Hi, Expert
My customer is asking how does PCM6260 TDM support 73.728 Mhz
384kHz×32bits×6ch=73.728MHz
Out put to external Audio chip via SDOUT TDM.
Your advice…